Organisms - Circuit design system

in development

Header International

Description

The international panel enables users to switch between country sites and — where relevant — change the language or regional norm context, right from the header. It makes DEHN’s global presence tangible and is primarily at home on the web presence (marketing and commerce sites).

In portals where country or regional context is meaningful (e.g., switching between country-specific standards or norms), an adapted version of the panel may be appropriate. Portals that only require a simple language switch, or where no internationalization is needed at all, should omit the panel — language switching in those contexts belongs in the footer and/or the user panel.


Use Cases


Usage

Rules & Guidelines

Trigger icon states:

The icon communicates the available feature scope before the panel is opened.

Panel variants:

1 — Full variant (multilingual site)

international header panel

2 — Reduced variant (single-language site)

international header panel without language switch

Country selection: When switching a country site, the user leaves the current site and is taken to the home page of the target site. This must be communicated clearly through the context of the selection list.

Language switcher: Changes the language within the same site. The lang attribute of the page must be updated programmatically after switching.

Responsive behaviour

The panel adapts in two steps, in line with the general header responsive behaviour.

Tablet: The panel retains its full layout — language switcher and tabbed region selection (Europe, Americas, Africa and M. East, Asia) — while adapting to the reduced available width. international header panel at tablet width

Mobile: The panel moves to the bottom of the mobile navigation overlay. The region tabs collapse into an accordion: each region becomes an individually expandable section, allowing users to navigate country links without horizontal tab navigation. The partner search teaser remains visible below the accordion. international header panel on mobile

Accessibility


Resources